TI E2E Community (Beta)
Welcome to the TI E2E (Engineer-to-Engineer) Community! We invite you to freely and openly interact with your peer Engineers, TI Engineers, and other experts in order to ask questions, share knowledge, explore ideas, and help solve problems.
More Search Options

BrandonAzbell

Schaumburg, IL
1,179 Posts

Shared Favorites

  • BrandonAzbell has not yet identified any favorite posts.
View all favorites

Shared Feeds

BrandonAzbell has not entered any shared feeds.

My Bio

BrandonAzbell has not entered a biography.

Announcements

My Activity

My Comments

pbpkb wrote help with CCStudio 4 bug!
on 16 Nov 2009 1:11 AM

I have an identical project that I can compile using CCStudio v3.3 and v4 using CGtools 5.2.1

  • builds without any problems
  • I can use the RAM linker file and run it in debug mode without any problems
  • when I use the Flash linker file it builds no problems
  • when I try flashing it works fine through CCStudio v3.3 but in v4 it crashes midway after erase due to an unexpected halt??

I can also take the output file from CC Studio v4 and load it onto a board using the CCStudio v3.3 programmer and it runs fine so the problem appears to be with the CCStudio v4 Flash API and the TMS320F2801.

Incidentally I have no problems running the code on a TMS320F2808 when compiled with the relevant memory map ofcourse.

Is there a way to change the Flash API for Code Composer v4?

oussama derbel wrote cc 2430db
on 16 Jul 2009 8:52 AM

HELLO

i want to program a timer with the cc 2430 db and the Z stack

i don't nów how to start because documentation is not available in the net.

so can you help me

THANK

Ousama

oussama derbel wrote cc 2430db
on 16 Jul 2009 8:52 AM

HELLO

i want to program a timer with the cc 2430 db and the Z stack

i don't nów how to start because documentation is not available in the net.

so can you help me

THANK

Ousama

brighenti wrote support in eZ430-RF2500 uart speed
on 26 Jun 2009 5:01 PM
Hey BrandonAzbell

You respond to a post in this forum about modifying the baud rate of TUSB in the emulator board of msp430RF2500 demokit. I would like to know how to modify the baud rate, it need a baud rate of 460800bps. I know that through the pins TPx is possible to rewrite the firmware of the Emulator Board.
Can You  help me please?

Thanks in advance

Best Regards
virendra jadav wrote Need help for ez430-rf2500 kit
on 19 May 2009 9:27 AM

Hello,

                   I am jadav virendra . I am studying in BE (electronics and communication). I make a project named wireless process control in my BE  last year. In this project for wireless communication I used two ez430-RF2500 kit. I give description of my project then I tell u a problem. In my project there are two station one is master and second is slave which are located in different locations. I attach the circuit diagram of master and slave unit in attachments.

                 In slave unit microcontroller 8051 read the temperature with help of temperature sensor LM35 and ADC 0808. Then send the data of temperature to the master unit via simpliciTI kit. master unit receive the data of temperature and send appropriate controlling command back to slave unit. Then slave unit receive this data and do action to increase or decrease the temp. with using fan .

                Here slave unit  microcontroller 8051 give data to simpliciTI  kit using UART (Tx-Rx pins ) I connect this pins to UART port of msp430f2274.same connection is made for master unit.

                Now  my problem is there I cant made program for msp430f2274 which both transmit and receive the data from or to the  8051 UART and then give or take it to cc2500 which connected with it via spi. And I also cant create protocol for my wireless protocol..

               I kindly request you to send a mail to  me  this transmit and receive program for ez430-rf2500 kit . this program is very necessary to complete my project so please help me. My e-mail address is jadavvirendra@yahoo.com.                                                          

                                                                                                                                                                                                                                                Yours faithfully

                                                                                                                                                                                                                                                 Jadav virendra                                                                           

ALL CONTENT AND MATERIALS ON THIS SITE ARE PROVIDED "AS IS". TI AND ITS RESPECTIVE SUPPLIERS MAKE NO REPRESENTATIONS ABOUT THE SUITABILITY OF THESE MATERIALS FOR ANY PURPOSE AND DISCLAIM ALL WARRANTIES AND CONDITIONS WITH REGARD TO THESE MATERIALS, INCLUDING BUT NOT LIMITED TO, ALL IMPLIED WARRANTIES AND CONDITIONS OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, TITLE AND NON-INFRINGEMENT OF ANY THIRD PARTY INTELLECTUAL PROPERTY RIGHT. NO LICENSE, EITHER EXPRESS OR IMPLIED, BY ESTOPPEL OR OTHERWISE, IS GRANTED BY TI. USE OF THE INFORMATION ON THIS SITE MAY REQUIRE A LICENSE FROM A THIRD PARTY, OR A LICENSE FROM TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI and its suppliers reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.