TI E2E Community (Beta)
Welcome to the TI E2E (Engineer-to-Engineer) Community! We invite you to freely and openly interact with your peer Engineers, TI Engineers, and other experts in order to ask questions, share knowledge, explore ideas, and help solve problems.
More Search Options

Binary file from CCS

rated by 0 users
Not Answered This post has 0 verified answers | 5 Replies | 3 Followers

Not Ranked
7 Posts
Community Member
Tobias Knutsson posted on 26 Jun 2009 10:23 AM

Hello,

I'm using the OMAP-L137 EVM Kit to run a GNU/Linux system and that is working fine. Now I would like to load a DSP-application into RAM and have the DSP execute it. My question is, is there a simple way of compiling a raw binary that I can place in RAM and execute? In essence, what I want to do is to capture the data that "File->Load Program" stores in RAM on the target, into a file that i can load into RAM from the Linux system running on the ARM CPU.

All Replies

Top 10 Contributor
2,298 Posts
Texas Instruments Employee

I believe you could do this with the hex conversion utility (hex6x.exe) with the -b option, though I am not sure this is well documented in SPRU186, I have seen it used with the UBL conversion to binary, the UBL build may make make a good reference for this sort of thing.

Tobias Knutsson:
In essence, what I want to do is to capture the data that "File->Load Program" stores in RAM on the target, into a file that i can load into RAM from the Linux system running on the ARM CPU.

This would be a different approach that may also work, you can save and load raw data on the target with the File -> Data... menu of CCS, I suppose if you knew where everything was being loaded by the .out file and it was all relatively contiguous that you could make a dump of the loaded image and restore it later, however I have not tried this.

Not Ranked
7 Posts
Community Member

Thank you, after examining ubl2bin.cmd from the ubl project I managed to create a compatible binary. Now my problem is how to release the DSP from reset. I have tried to power up power domain 1 by writing 1 to the NEXT field in PDCTL1 and writing 0x00000103 (Enable state and de-assert local reset) to MDCTL15 and then written a 2 to PTCMD but reading from MDSTAT15 reveals the DSP to remain in reset. However, looking in CCS the DSP is reported to have both power and clock on and not in reset. What am I missing?

Not Ranked
7 Posts
Community Member

The thing is that I do not want to have a custom application in the DSP ROM. There must be some way to release the DSP from reset, right?

Other then transitioning from SwRstDisable state to Enable state and de-asserting local reset, what are the steps required to release the DSP from reset?  

Not Ranked
7 Posts
Community Member

Ok, problem fixed.

It turns out that you do not have to do anything else. You do however need to enable for example the gpio module if your test application is the led test program. I was trying my code in u-boot, at which point these modules had not been initialized yet. If I booted Linux first, it all worked fine. The thing that confused me was that connecting to CCS and then disconnecting again apparently enables all modules.

Page 1 of 1 (6 items) |

ALL CONTENT AND MATERIALS ON THIS SITE ARE PROVIDED "AS IS". TI AND ITS RESPECTIVE SUPPLIERS MAKE NO REPRESENTATIONS ABOUT THE SUITABILITY OF THESE MATERIALS FOR ANY PURPOSE AND DISCLAIM ALL WARRANTIES AND CONDITIONS WITH REGARD TO THESE MATERIALS, INCLUDING BUT NOT LIMITED TO, ALL IMPLIED WARRANTIES AND CONDITIONS OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, TITLE AND NON-INFRINGEMENT OF ANY THIRD PARTY INTELLECTUAL PROPERTY RIGHT. NO LICENSE, EITHER EXPRESS OR IMPLIED, BY ESTOPPEL OR OTHERWISE, IS GRANTED BY TI. USE OF THE INFORMATION ON THIS SITE MAY REQUIRE A LICENSE FROM A THIRD PARTY, OR A LICENSE FROM TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI and its suppliers reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.