TI E2E Community (Beta)
Welcome to the TI E2E (Engineer-to-Engineer) Community! We invite you to freely and openly interact with your peer Engineers, TI Engineers, and other experts in order to ask questions, share knowledge, explore ideas, and help solve problems.
More Search Options

Need Schematic for PTH08D110 Module

rated by 0 users
Not Answered This post has 0 verified answers | 7 Replies | 4 Followers

Not Ranked
2 Posts
Community Member
Elden Crom posted on 27 Jan 2009 1:07 PM

--or the spec for the module

The PTH08D110 is a part on the 'EightChBuck-DCDC-SCH.pdf' from sprc678 (In the BOM for the TMDSDCDC8KIT, it's listed as 'TI to provide').  But I don't know what's inside.  And google and the TI site don't recognize the part number. My questions are,

a) How is the current measured, can it measure negative? Is it across the highside or from the lowside fet?

b) What happens when the Inhibit is driven low.

c) What is SRE?

I would like to use this dev kit to drive a three phase sensorless motor. To do so I need to allow one phase to float, ie both highside and lowside fett need to be off, so that I can read the voltage generated by that winding. Thus, I think I need to wire the Inhibt to a GPIO, assuming that I won't blow anything up.

 

 I think I found My answer....the part number in the schematic is wrong it's actually a PTD08A010W.

 

All Replies

Not Ranked
3 Posts
Texas Instruments Employee

Yes, the part number is PTD08A010W.  This is a 10A power train module that uses a UCD7230 as a driver.  This driver has an integrated current sense amplifier.

a) This module uses the DCR of the inductor to measure current.  The UCD7230 has a gain of ~48X.  It also applies a 0.6V bias to the current mesurment so that it can measure negative current.

b) The inhibit input when driven low will turn off the output and will cancel the PWM and SRE input operation to the UCD7230.

c) SRE is the Synchronous Rectifier Enable pin.  When this logic input is high, then the synchronous FET is operational allowing the module to both sink and source current.  When this input is low then the module can only supply current.

This module is intended to be used with either a member of the UCD911X or UCD92XX family of digital controllers.

Let me know if you need more information. 

Not Ranked
2 Posts
Community Member

 

I'm not sure what happend to my other reply but it appears to have not posted.

What I need is a similar pin out to the PTD08A010W (Temp, Current, PWM in, etc) but with an input range of about 40 to 42 Volts, with an output of 5 to 38 Volts....or simply a 0 to 28V output with current monitoring extending 5 volts on either side of the rails.

If the module does not exist (the PTN04050C is getting closer, voltage and current wise, but futher away function wise), is there a chip similar to the UCD7230 that has a wider common mode voltage for current sense?

(need around 8k to 10k units)

 

Not Ranked
4 Posts
Texas Instruments Employee

Mr. Elden Crom:

I reviewed you request for  an hihg voltage  PTD08A010 with UCD7230. Thr e are no plans to develop a module with thsi capability.

However, I have attached a link to a power solution, using the TPS54160 IC.1.5A wide input voltage (60V to lower voltages to 58V output  voltage

http://focus.ti.com/docs/prod/folders/print/tps54160.html

Regards

Tom Guerin

Not Ranked
9 Posts
Community Member

Dear Tom,

In my project ,power stage is controled by UCD7230. vin =15volt,double phase vout,FS=1MHZ,L=0.5uH,C=470uf*5+47uf*10,I want to get a adjustable Vout of 0 to 12volt. in the course of regulating, ofen burn down the low side MOSFET,ucd7230 is hot too, it will be better when configure single phase.Could you share the reference circuit of ucd7230 and reference configure with me,Could you share me the  PTH08D110 SCH? thanks !

Not Ranked
4 Posts
Texas Instruments Employee

Mr. Changling WU :

I receved this  e-mail concerning the PTD08A010  .There are many concerns about this high frequency  operation an   voltage range. The UCD 7230 is limited  0.7V to 3.6V Vout .THePTD serise limited to 0.7V to 3.6V Vout. See teh prodcut UCD 7230 wEB site for details.

This includes the  minimum maximum Vout data  and      http://focus.ti.com/docs/prod/folders/print/ucd7230.html pages under propagation  delay and maximum Vin to Vout .

Regards

Tom Guerin

Not Ranked
9 Posts
Community Member

Dear Tom,

I can not find any information that ucd7230 can not support 12volt vout in spec. in our project ,the power stage that engaged in ucd7230 can already support 12volt vout ,but the configure is single phase , As i want get more current output (about 50A),so i need double phase configure ,but it is not stable sometime can not get any vout, MOSFET was often  burned down ,by the way ,ucd9240 is unable to sense correctly current of powr stage,what configuration does the ucd9240 need? do you have any suggestion for me? thank you!

 

 

Not Ranked
4 Posts
Texas Instruments Employee
  1. Dear Changling Wu:

Thansk for the-mail.

The UCD specification on page 5 under maximum Vin  of 15V  has the analog or Vout  limited 0.7V to 3.6V. It cannot accept vout of greater than  3.6V Vout.

http://focus.ti.com/docs/prod/folders/print/ucd7230.html. See the  link with data on the  UCD7230.

best regards

Tom Guerin

 

 

 

Page 1 of 1 (8 items) |

ALL CONTENT AND MATERIALS ON THIS SITE ARE PROVIDED "AS IS". TI AND ITS RESPECTIVE SUPPLIERS MAKE NO REPRESENTATIONS ABOUT THE SUITABILITY OF THESE MATERIALS FOR ANY PURPOSE AND DISCLAIM ALL WARRANTIES AND CONDITIONS WITH REGARD TO THESE MATERIALS, INCLUDING BUT NOT LIMITED TO, ALL IMPLIED WARRANTIES AND CONDITIONS OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, TITLE AND NON-INFRINGEMENT OF ANY THIRD PARTY INTELLECTUAL PROPERTY RIGHT. NO LICENSE, EITHER EXPRESS OR IMPLIED, BY ESTOPPEL OR OTHERWISE, IS GRANTED BY TI. USE OF THE INFORMATION ON THIS SITE MAY REQUIRE A LICENSE FROM A THIRD PARTY, OR A LICENSE FROM TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI and its suppliers reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.