<?xml version="1.0" encoding="UTF-8" ?>
<?xml-stylesheet type="text/xsl" href="http://community.ti.com/utility/FeedStylesheets/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:slash="http://purl.org/rss/1.0/modules/slash/" xmlns:wfw="http://wellformedweb.org/CommentAPI/"><channel><title>Power Over Ethernet</title><link>http://community.ti.com/forums/103.aspx</link><description>Discuss the IEEE802.3af (Power Over Ethernet) standard and its related devices, applications, uses, problems, stability, solutions and component selection.</description><dc:language>en</dc:language><generator>CommunityServer 2008.5 SP2 (Debug Build: 40407.4157)</generator><item><title>Reference design for TPS23754 3.3V output</title><link>http://community.ti.com/forums/thread/49120.aspx</link><pubDate>Tue, 17 Nov 2009 09:55:50 GMT</pubDate><guid isPermaLink="false">35ded035-4cd5-4bbd-851f-937553e04a39:49120</guid><dc:creator>SanchoPancho</dc:creator><slash:comments>1</slash:comments><comments>http://community.ti.com/forums/thread/49120.aspx</comments><wfw:commentRss>http://community.ti.com/forums/commentrss.aspx?SectionID=103&amp;PostID=49120</wfw:commentRss><description>&lt;p&gt;Hi,&lt;/p&gt;
&lt;p&gt;Is there a reference design for TPS23754 for 3.3V output? There is only reference designs for 5V and 12V outputs.&lt;/p&gt;
&lt;p&gt;&amp;nbsp;&lt;/p&gt;
&lt;p&gt;tnx&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;</description></item><item><title>IEEE 802.3af standard problem using the TPS23750PWP</title><link>http://community.ti.com/forums/thread/40971.aspx</link><pubDate>Fri, 25 Sep 2009 15:19:56 GMT</pubDate><guid isPermaLink="false">35ded035-4cd5-4bbd-851f-937553e04a39:40971</guid><dc:creator>Jelle</dc:creator><slash:comments>1</slash:comments><comments>http://community.ti.com/forums/thread/40971.aspx</comments><wfw:commentRss>http://community.ti.com/forums/commentrss.aspx?SectionID=103&amp;PostID=40971</wfw:commentRss><description>&lt;p&gt;Hello,&lt;/p&gt;
&lt;p&gt;I have a problem with my currently designed PD device. I used at this moment the spare lines for getting power for my pd device. The problem is that a Endpoint (end-span)&amp;nbsp;switch needs to see the pd on the spare-lines and &lt;strong&gt;data-lines.&lt;/strong&gt; To make our system accept power from the datalines isn&amp;#39;t possible because the transformer isn&amp;#39;t suitable for POE current.&lt;/p&gt;
&lt;p&gt;The only way to let the switch believe that there is a correct PD device present, is to place a 25k Ohm resistor between the transformer points of the data lines. But is this possible and does this work or is this allowed??&lt;/p&gt;
&lt;p&gt;Hopefully you can answer my question.&lt;/p&gt;
&lt;p&gt;Thanks,&lt;/p&gt;
&lt;p&gt;Jelle&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;</description></item><item><title>Output Voltage Range of PoE controllers with built-in DC/DC converters</title><link>http://community.ti.com/forums/thread/25723.aspx</link><pubDate>Wed, 10 Jun 2009 08:11:28 GMT</pubDate><guid isPermaLink="false">35ded035-4cd5-4bbd-851f-937553e04a39:25723</guid><dc:creator>Johnny T</dc:creator><slash:comments>1</slash:comments><comments>http://community.ti.com/forums/thread/25723.aspx</comments><wfw:commentRss>http://community.ti.com/forums/commentrss.aspx?SectionID=103&amp;PostID=25723</wfw:commentRss><description>&lt;p&gt;Hi.&lt;/p&gt;
&lt;p&gt;I&amp;#39;m normally not designing power-related circuitry, but now I&amp;#39;m considering the using the TPS23754 in a design. I have tried to read the spec, but I&amp;#39;m still not sure about the output levels and how it&amp;#39;s adjusted.&lt;/p&gt;
&lt;p&gt;I need to generate a +24V system voltage (1A max current), from the ethernet cable. Is this voltage level achievable, and what transformer should I use?&lt;/p&gt;
&lt;p&gt;I&amp;#39;m planning on implementing this feature on a Gigabit LAN. Do you seee any problems with that?&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;</description></item><item><title>doubt related to my project</title><link>http://community.ti.com/forums/thread/12947.aspx</link><pubDate>Tue, 24 Feb 2009 14:02:12 GMT</pubDate><guid isPermaLink="false">35ded035-4cd5-4bbd-851f-937553e04a39:12947</guid><dc:creator>nikunj shah</dc:creator><slash:comments>1</slash:comments><comments>http://community.ti.com/forums/thread/12947.aspx</comments><wfw:commentRss>http://community.ti.com/forums/commentrss.aspx?SectionID=103&amp;PostID=12947</wfw:commentRss><description>&lt;p&gt;Introduction: &lt;br /&gt;Hello sir, myself Nikunj, trying to make project on &amp;ldquo;ETHERNET ENABLED UNIVERSAL CONTROLLER&amp;quot; it means that it would be monitoring (sensing) and controlling various parameters at a time and also on a single cable. In my project I&amp;rsquo;ve taken thermocouple, PT-100 RTD, 1-5 volt signal source and 4-20 mA current signal source and would be providing these all signal conditioning to convert them into 1-5V signal. Then I would be multiplexing and converting them to digital signal by ADC with inbuilt MUX and transmitting data to microcontroller which I would be programming to display data on local LCD and also on a PC for a front end purpose. I would be providing 6push buttons to make different settings such as &amp;#39;enter, up, down, shift left, shift right, auto- manual mode purpose&amp;#39;. I&amp;rsquo;ll be implementing software temperature compensation for thermocouple and RTD in program itself. I&amp;#39;ll be implementing PID algorithm for controlling purpose of parameters at their set point and outputting these data on DAC to D_MUX to 4 different controlling elements such as valves. I&amp;#39;ve also provided ETHERNET IC interfacing with microcontroller. &lt;br /&gt;&lt;br /&gt;PROBLEM:&lt;br /&gt;Now the problem I&amp;#39;m facing is the selection of components, especially microcontroller because ADC which I&amp;rsquo;ve selected has serial output and DAC has serial input, PC also has communication via serial port. If I think, Ethernet IC would also be having serial communication. How would I interface all these components on microcontroller having one serial port? Also I need to interface LCD and switches beyond that. So if u please suggest me any microcontroller for this purpose that would be able to interface all these devices and if u suggest name of each components from TI and circuit diagram of the whole interfacing, it would be very thank full to you. I was wishing to select TLK1201ARCP ETHERNET IC and ADS1256 ADC with inbuilt MUX from TI. &lt;br /&gt;REQUEST:&lt;br /&gt;right now I&amp;#39;m having exams which will be over by the end of January. So if u provide me the whole circuit so that I can give it for fabrication by this time and after that I can focus on programming it would be very thank full to you.&lt;br /&gt;&lt;br /&gt;Yours sincerely,&lt;br /&gt;NIKUNJ SHAH&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;</description></item></channel></rss>