TI E2E Community (Beta)
Welcome to the TI E2E (Engineer-to-Engineer) Community! We invite you to freely and openly interact with your peer Engineers, TI Engineers, and other experts in order to ask questions, share knowledge, explore ideas, and help solve problems.
More Search Options

i2c boot

rated by 0 users
Not Answered This post has 0 verified answers | 20 Replies | 3 Followers

Not Ranked
15 Posts
Community Member
Michael Markov posted on 29 Jun 2009 8:36 AM

Hello. I have a problem with making EEPROM image from *.out file. Some utilites make text file. Of cause EEPROM contents binary data after loading with CCS. My TMS is - C6455. Can anybody tell me how to create binary which I can save to EEPROM 0x0 address?

All Replies

Top 10 Contributor
2,298 Posts
Texas Instruments Employee

Though this may not have a great answer, there is another thread here that has a couple of ideas for this sort of thing.

Not Ranked
15 Posts
Community Member

I solve this problem by writing tool that converts ccs file in compatible binary. And it works.

My next problem is i2c slave boot. Cause my code have size more than on-board EEPROM size. How can I solve this problem?

Top 10 Contributor
2,298 Posts
Texas Instruments Employee

I am glad to hear your tool works.

Michael Markov:
My next problem is i2c slave boot. Cause my code have size more than on-board EEPROM size. How can I solve this problem?

Assuming your I2C EEPROM cannot be made larger the first thing I would do is try out some reduced code size build options to see if you can make your code size small enough to fit, in particular --opt_for_space=3 and turning off the debug information with --symdebug:none, these options and more are discussed further in SPRU187. If it still cannot fit in your EEPROM than you would probably have to increase the size of the EEPROM or move to another boot method that has enough space for your application code.

Not Ranked
15 Posts
Community Member

Bernie Thompson:
I am glad to hear your tool works.
Thanks :-)

Bernie Thompson:
Assuming your I2C EEPROM cannot be made larger the first thing I would do is try out some reduced code size build options to see if you can make your code size small enough to fit, in particular --opt_for_space=3 and turning off the debug information with --symdebug:none, these options and more are discussed further in SPRU187. If it still cannot fit in your EEPROM than you would probably have to increase the size of the EEPROM or move to another boot method that has enough space for your application code.

I think our code will be lager then on-booard EEPROM. My question is: If I understand slave i2c boot mode right? I suggest that this mode allows my code can be loaded without EEPROM memory. I want to load this from other IIC device passing EEPROM.

Can I do so? If yes. How much can be this code (Is it restricted by EEPROM size)?

If restricted, an idea is in using second level bootloader, but we will not have EEPROM on our board. Sorry for my English. Do you understand me?

Top 10 Contributor
2,298 Posts
Texas Instruments Employee

Michael Markov:
I think our code will be lager then on-booard EEPROM. My question is: If I understand slave i2c boot mode right? I suggest that this mode allows my code can be loaded without EEPROM memory. I want to load this from other IIC device passing EEPROM.

It seems it was designed around having multiple C6455 devices booting off of the same EEPROM by designating all to be slaves except for one master, however I see no immediate reason that you could not simulate an EEPROM from another processor on your board that has an I2C interface to allow for booting a larger amount of code than your own EEPROM can hold.

Michael Markov:
Can I do so? If yes. How much can be this code (Is it restricted by EEPROM size)?

This is certainly worth trying, though I have not seen it done myself, the code can be as large as your I2C addressing allows for, and looking at the boot loader manual it seems it is using two 16 bit addresses so you should have 32 bits of address space or 2^32 bytes.

Not Ranked
15 Posts
Community Member

Bernie Thompson:
It seems it was designed around having multiple C6455 devices booting off of the same EEPROM by designating all to be slaves except for one master, however I see no immediate reason that you could not simulate an EEPROM from another processor on your board that has an I2C interface to allow for booting a larger amount of code than your own EEPROM can hold.

This is certainly worth trying, though I have not seen it done myself, the code can be as large as your I2C addressing allows for, and looking at the boot loader manual it seems it is using two 16 bit addresses so you should have 32 bits of address space or 2^32 bytes. I can'not find docs about it.

I think about data structure. EEPROM contaings data in 128 bit blocks and that data are read respectively block-by-block. If I will use i2c slave boot, what have I do? (use boot table splitted in 128 bit blocks or transfer boottable without splitting). Bootloader manual discribe i2c slave boot not well.

Really i2c allows address 2^33 bytes. It is enough for second level bootloader, but programm doesn't work.
 If you don't understand, I send data to IIC from the other board.

 

Thanks for much help from you.

Top 200 Contributor
44 Posts
Texas Instruments Employee

Michael,

I didn't see a reference anywhere above to the following link, which describes I2C boot and gives an example.  The zip file contains utilities to convert your .out file to a boot table that can be loaded in I2C slave boot mode.

 

http://focus.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=spraae9

 

Attached is some additional reference code for I2C slave boot process. There is a big endian and little endian examples, so use the appropriate one (LE uses I2Cboot and simple_le_2; BE uses I2Cboot_be and simple_be_2; both use Utilities). Each has a batch file with appropriate steps and switches to use. The starting point is the assembly file simple.s which was used to generated simple_him.out. Once you have the .out file, you can run the batch file I2Cboot.bat. The final output file of the batch run (simple.i2c.ccs) contains the data bits that would be sent in the DATA field of the 7-bit addressing mode I2C serial format. Notice that the simple.i2c.ccs is the exact same for le and be after the appropriate switches and executables are run. As you mentioned, the simple.i2c.ccs file data would need to be modified as shown below since the data can only be sent over in max 128B blocks, so it will have to be partitioned appropriately for larger boot table transfers. This example boot table can be sent in one block transfer.

 

Format like this:

Start, Slave add = 04, R/W=0, 0x00, 0x06, 0x00, 0x00, 0x00, 0x01, Stop Now send the boot table..

Start, Slave add = 04, R/W=0, 0x00, 0x34, 0x28, 0xd5, 0x00, 0x81, 0x00, 0x00, 0x00, 0x00, 0x00, 0x20, 0x00, 0x81, 0x00, 0x00, 0x00, 0x99, 0xa2, 0x28, 0x00, 0x88, 0x91, 0x68, 0x00, 0x02, 0xa1, 0x20, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, Stop

 

Output of .ccs file format

1651 1 10000 1 d - Delete this

0x003428d5

0x00810000

0x00000020

0x00810000

0x0099a228

0x00889168

0x0002a120

0x00000000

0x00000000

0x00000000

0x00000000

0x00000000

0x00000000

 

 

This simple boot table simply loads a register and waits.  Although I would not advise it because of boot time, I've known of complete programs (>1MB) loaded through I2C interface to work.

Hope that helps,

Travis

 

5228.I2C.zip

Not Ranked
15 Posts
Community Member

tscheck, Thank you for your reply. I haven't seen your archive, but I already had loaded program by to ways.

For beginning. I have made css-file with those utilites. Then using my own utilite to convert ascii css-file to hex data which must be in eeprom.

For second way I convert to hex btbl-file.

First way. I used i2c interface to transmit data in TMS EEPROM, than default bootloader in i2c master mode loads program.

Second one. I have written so-called second level bootloader. It receives program code and data from the other device and load its in to memory as it needs. Then I call an entry point.

Can you tell me, default bootloader is using 128b blocks not in case of EEPROM structure? May I use the default bootloader in i2c slave boot mode to read not from EEPROM but from my 'other device' directly?

One qustion more. When I load example program whis led blinking it works.  When I load my own program with "printf("Hello world")" Smile, printf function doesn't works. When I use debug throuth the asm code i have seen that all functions that usually called by printf have been called, but I do not see it in the Code Composer Studio.

 

Thank you.

Top 200 Contributor
44 Posts
Texas Instruments Employee

Just to be clear, the block size limitation is 128Bytes not bits.  To answer your question, yes, even in I2C slave mode, the max 128B block size must be used.  The I2C default slave boot mode relies on an external device to transfer data to the slave DSP through the I2C interface.  It is not a read operation like the I2C master boot mode.  This external master ('other device') could be another DSP or FPGA for example.  Any device that can properly operate as a I2C master should work.

 

Regarding the printf issue, I believe your problem is the sequencing and timing involved.  When you boot, you reset the device, at which time you can't connect to it via Code Composer Studio.  So if you boot your program and CCS isn't connected at the time it is trying to output the printf statement, you won't see it.  If you add a long timing loop, say 20seconds, before you call the printf, then that may give you enough time to attach CCS and see your message.

Let me know if that works so we can verify the answer.

Regards,

Travis

Not Ranked
15 Posts
Community Member

tscheck:

Regarding the printf issue, I believe your problem is the sequencing and timing involved.  When you boot, you reset the device, at which time you can't connect to it via Code Composer Studio.  So if you boot your program and CCS isn't connected at the time it is trying to output the printf statement, you won't see it.  If you add a long timing loop, say 20seconds, before you call the printf, then that may give you enough time to attach CCS and see your message.

Let me know if that works so we can verify the answer.

I have the other opinion.

Sequence.

In CSS I load my bootloader to TMS with JTAG. Then I recieve code of the required program (int other memory, loader works in IRAM program in DDR2) and call entry point. Connection to CCS is not lost, I can toggle breakpoints for example in asm-code. May be problem in addresses? Led blinking example is in IRAM, but I was lucky because new code hasn't overwritten bootloader code. I already have tried to use Delay Loops without result.

Not Ranked
15 Posts
Community Member

One more question. I want to use bootloader i2c slave mode. Master is the FPGA connected to tms. What address on i2c bus must I use to write boot parameters and boot table.

When I use address 0x1 or 0xA for example and check i2c line with the oscillograph I see normal address package on the oscillograph screen. But the data sending certanly fails (cause there is no device with such address on bus, I think). When I send data on address 0x0 (AFAIK broadcast), oscillograph displays strange behavour. IAE no byte send is successful.

Top 200 Contributor
44 Posts
Texas Instruments Employee

The i2c address for the DSP is given in the formatting example I showed above, 0x04.

Regards,

Travis

Not Ranked
15 Posts
Community Member

Thanks. Writing to 0x04 address is successful.

Now, I have a question about boot parameters format. Is it only example?

tscheck:

Start, Slave add = 04, R/W=0, 0x00, 0x06, 0x00, 0x00, 0x00, 0x01, Stop Now send the boot table..

Bootloader user's guide contents the description of boot parameters table. It's size is 26 byte. First byte is a length of itself for example. You give me only six bytes in the example. What I don't understand incorrectly?

Not Ranked
15 Posts
Community Member

Hello, Travis. I can load the DSP Program with your boot parameters table example!

My next task is loading program that using leds. My question is in the init process. When I'm connecting to DSP with Code Composer Studio, my program (it's in assembler just writing to the leds address) works properly. Without ccs I need to setup memory map and other initialization features. How can I do it. Can you tell me what documentation can I read about it. Thanks a lot. You have already helped me much.

Page 1 of 2 (21 items) 1 2 Next > |

ALL CONTENT AND MATERIALS ON THIS SITE ARE PROVIDED "AS IS". TI AND ITS RESPECTIVE SUPPLIERS MAKE NO REPRESENTATIONS ABOUT THE SUITABILITY OF THESE MATERIALS FOR ANY PURPOSE AND DISCLAIM ALL WARRANTIES AND CONDITIONS WITH REGARD TO THESE MATERIALS, INCLUDING BUT NOT LIMITED TO, ALL IMPLIED WARRANTIES AND CONDITIONS OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, TITLE AND NON-INFRINGEMENT OF ANY THIRD PARTY INTELLECTUAL PROPERTY RIGHT. NO LICENSE, EITHER EXPRESS OR IMPLIED, BY ESTOPPEL OR OTHERWISE, IS GRANTED BY TI. USE OF THE INFORMATION ON THIS SITE MAY REQUIRE A LICENSE FROM A THIRD PARTY, OR A LICENSE FROM TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI and its suppliers reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.