Hello All,
I am using SimpliciTI version 1.0.6 using the eZ430RF2500 board.
I am also implementing acknowledgments in the application layer for communication between one AP and multiple EDs.
However I am getting a stack overflow error in the AP. Can anyone tell me how to get rid of this problem?
When does a stack overflow error happen?
Regards,
Sharwari
Stack overflow occurs when your stack (the dynamic memory structure that holds function variables, return addresses, etc.) grows in size and spills over into RAM that is holding program variables. This commonly happens when you have long chains of function calls and/or variables using too much RAM. Probably a crappy definition, but eh, I'm sure you can find a better one with not too much searching.
I assume you mean the linker is giving you some sort of stack overflow error? I'm not aware of any sort of run-time stack-overflow error message...don't think that's possible.
I had problems with stack overflow on my AP (v1.0.5 SimpliciTI). The MSP430F2274 only has 1 kB of RAM. Depending on the number of end devices you have and the size of your input/output queues, you can use this 1 kB up very quickly. I think the stack defaults somewhere between 64 and 128 kB with Code Composers. You can set it in the linker options under project preferences. If the RAM required for you I/O queues invades upon the stack's space, I think the linker will complain.
My stack overflow led to cryptic behavior and dropped SimpliciTI packets.
I decreased the size of my input/output queues and limited the number of end devices that could connect to the AP at any one time to 3. You can see my memory mappings here: http://e2e.ti.com/forums/p/3919/14650.aspx#14650
Hello,
Thanks for your reply.
I just have one question to ask.
How did you restrict the number of EDs that can join an AP at any one time to be 3? What was the maximum number of EDs that you had in your application?
Also I am sure what you mean by "queue size"? Does the number of EDs affect the stack size? If so, how and why?
Thanks
Normal 0
I don't know what that Normal 0 means...I imported this from a .doc file and it screwed with all my formatting and added that.
I don't think the number of end devices affects memory usage in a very significant way directly. Sorry that my words seemed to convey that. The access point will store connection information for every end device, but I think the number of bytes required for this is insignificant when compared to the queues. Certainly seems so by investigating my memory mappings. However, the number of end devices you have connected to the AP and whether these are polling end devices or not should influence the size of your queues. Specifically, the output queue stores messages meant for polling end devices. Say you have 5 polling end devices. You’d want an output queue at least 5 messages long, so you could send out a message to each device at the same time, probably longer. This was how I was drawing the connection between number of end devices and memory usage. If you have fewer polling end devices, you can decrease the size of your output queue and save memory.
For setting the number of end devices, I assume you've seen some of the TI-provided sample code. They provide two configuration header files for setting device and network parameters. I think the names are smpl_config.h and smpl_nwk_config.h, but I'm not exactly sure. You edit the number of end devices by defining the parameter NUM_END_DEVICES (again, exact name may be a little different, I'm working off memory). If you’re using the AP as a data hub, it will only let the number of end devices defined by NUM_END_DEVICES join the network. If you’re not using the access point as a data hub, perhaps this information isn’t relevant.
In these configuration files, you also set the input and output queue sizes as well as the maximum application payload. The queue sizes define the number of SimpliciTI messages that the queue can hold. If you don’t like the name queue, think of it as a message buffer instead. The MAX_APP_PAYLOAD parameter defines the size of these messages, but doesn't account for the couple bytes of overhead. To reduce memory used by the queues, reduce the maximum app payload and/or the queue sizes. Roughly, the number of bytes required by a queue is PAYLOAD * QUEUE_SIZE.
Also, there are some protocol docs that you may want to check out, if you haven’t already. I think installing the protocol via the executable in swrc099c.zip will copy all the docs onto your computer for you. There’s a detailed SimpliciTI protocol doc, an API guide doc, etc. If you plan on using SimpliciTI for much longer, I suggest you read them in full. They’re rather short as technical docs go.
ALL CONTENT AND MATERIALS ON THIS SITE ARE PROVIDED "AS IS". TI AND ITS RESPECTIVE SUPPLIERS MAKE NO REPRESENTATIONS ABOUT THE SUITABILITY OF THESE MATERIALS FOR ANY PURPOSE AND DISCLAIM ALL WARRANTIES AND CONDITIONS WITH REGARD TO THESE MATERIALS, INCLUDING BUT NOT LIMITED TO, ALL IMPLIED WARRANTIES AND CONDITIONS OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, TITLE AND NON-INFRINGEMENT OF ANY THIRD PARTY INTELLECTUAL PROPERTY RIGHT. NO LICENSE, EITHER EXPRESS OR IMPLIED, BY ESTOPPEL OR OTHERWISE, IS GRANTED BY TI. USE OF THE INFORMATION ON THIS SITE MAY REQUIRE A LICENSE FROM A THIRD PARTY, OR A LICENSE FROM TI.
Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI and its suppliers reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.