Hi,
Regarding the linked post it was mentioned that there it will be worked on a Python script to parse the data from the mmWave Demo coming from the UART.
Is this already published? I did not fin one.
I need it to for the data...
Read more.TI E2E™ design support forums are an engineer’s go-to source for help throughout every step of the design process.
Our engineers answer your technical questions and share their knowledge to help you quickly solve your design issues.
Start by searching thousands of existing answers to see if the solution to your problem is already online.
Log in or create a free myTI account to post a new question and connect with our engineers.
For non-design-related questions such as ordering semiconductor parts and tools, contact our customer support center where you can open a support ticket, chat with us 24 hours a day, Monday through Friday; or call the TI support team.
Hi,
Regarding the linked post it was mentioned that there it will be worked on a Python script to parse the data from the mmWave Demo coming from the UART.
Is this already published? I did not fin one.
I need it to for the data...
Read more.Hi,
I am testing this load switch and imported the .LIB file from ti.com into ADS, but I am not getting any changing results on Vout. There is no documentation that verifies which pin on the SPICE model corresponds to which pin on...
Read more.Hi Shreyas,
S-param extraction is a feature in ADS, but needs a properly functioning load switch in order to work. The help I need is really something similiar to John Miller's in this thread:
I tried to recreate his fix, but had no luck. Is there...
Read more.Lysny,
We can't provide support for Keysight ADS, we do not have access to this software and officially only support the use of our models with TINA and Cadence PSIPCE (TI version).
I would suggest to use PSPICE for TI but it doesn't support the...
Read more.Tool/software: Code Composer Studio
Hi, I am developing a datalogger that collects information from several sensors with different protocols such as I2C, UART, 1-Wire, etc, and then saved in an I2C memory. Then, it transfers...
Read more.Hello Jesus,
Are you trying to make the different ports support multiple sensors then figure out which sensor is connected to that port?
Luke
Hi,
We'd like to sequence the following chirp configuration in a cascaded AWR1243P design:
CHIRP1 x 512 TX0-MASTER ------> CHIRP2 x 512 TX1-SLAVE -----> CHIRP3 x 512 TX2-SLAVE
For example, master chirp configuration looks...
Read more.Hello,
Glad that you are able to get the correct LVDS signal.
You need to have same no. of chirp in frameData.subframeDataCfg[x].totalChirps to get all the chirp data over CSI2/LVDS, that you did this time correctly.
Now for your other question on Tx...
Read more.Hi,
Accoding to
https://e2e.ti.com/support/sensors/f/1023/t/686001
LVDS valid is only high for the first frame in an apparently multiple frame configuration.
We're following a sub-frame configuration (total of 3) for a master...
Read more.Hi Vivek,
Many thanks for your reply. You're correct, we are not seeing the second and third subframes in either chips.
This is our triggering setting:
if (deviceMap == RL_DEVICE_MAP_CASCADED_2) { advFrameCfgArgs.frameSeq.triggerSelect = 2;...
Hello,
the master should be in SW triggered mode and slave device in HW triggered mode. The SYNC OUT of the master needs to be connected to the SYNC IN pin of the slave so that it receives the SYNC pulse and triggers the chirps.
Regards,
vivek
Hello Max,
There is not a public Python script to parse the data. However, please refer to the attached slide deck for data structure information. Additionally, this version of the Demo Visualizer enables logging of the output to a CSV file.
If there...
Read more.