TI E2E Community (Beta)
Welcome to the TI E2E (Engineer-to-Engineer) Community! We invite you to freely and openly interact with your peer Engineers, TI Engineers, and other experts in order to ask questions, share knowledge, explore ideas, and help solve problems.
More Search Options

OPA1632 Vocm pin

rated by 0 users
Answered (Verified) This post has 1 verified answer | 3 Replies | 1 Follower

Not Ranked
6 Posts
Community Member
peranders posted on 9 Oct 2009 7:29 AM

Hi!

 

OPA1632, pin 2, what is the input characteristics of this input? Can't find anything in the datasheet.

Have I understood it right: This input makes the outputs be centered around the voltage at this pin?

/Per-Anders

Answered (Verified) Verified Answer

Top 50 Contributor
103 Posts
Community Member
Verified by Matt

Hi Peranders,

You are right. But there is a little bit more to it.

Vocm sets the output common mode voltage, the voltage level around which the output voltage is centred.

By default it is set to Vcc/2 where Vcc is the supply voltage, if it is required to be at the same level, then Vocm should be left unconnected.

If you require a dc shift in the output voltage ,then you need to apply the required voltage level from an external voltage source to the Vocm pin. It also requires a 0.1uF decoupling capacitor to filter out any high-frequency noise.

Regards,

Sid

All Replies

Top 50 Contributor
103 Posts
Community Member
Verified by Matt

Hi Peranders,

You are right. But there is a little bit more to it.

Vocm sets the output common mode voltage, the voltage level around which the output voltage is centred.

By default it is set to Vcc/2 where Vcc is the supply voltage, if it is required to be at the same level, then Vocm should be left unconnected.

If you require a dc shift in the output voltage ,then you need to apply the required voltage level from an external voltage source to the Vocm pin. It also requires a 0.1uF decoupling capacitor to filter out any high-frequency noise.

Regards,

Sid

Not Ranked
6 Posts
Community Member

Bump, this question. TI must have specs somewhere about this input?

/Per-Anders

Top 50 Contributor
103 Posts
Community Member
Sid replied on 28 Oct 2009 12:49 AM

Hi peranders,

Actually Vocm just sets the DC voltage level around which the OUTPUT voltage is centred.

The peak to peak level of output voltage is the same. Its just that this output voltage is offset by the voltage given to Vocm. This offset voltage should not need any specifications because it mainly depends on what device you are using at the output of OPA1632. You can have the dc offset as 0V, 1V, 5V, 10V ,etc.. as long as it is sustainable by the device to which this output voltage is fed. The peak to peak output voltage is still the same.

So, I think the specifications are not mentioned because they can be variable depending on the output device.

Hope this helps.

Regards,

Sid

Page 1 of 1 (4 items) |

ALL CONTENT AND MATERIALS ON THIS SITE ARE PROVIDED "AS IS". TI AND ITS RESPECTIVE SUPPLIERS MAKE NO REPRESENTATIONS ABOUT THE SUITABILITY OF THESE MATERIALS FOR ANY PURPOSE AND DISCLAIM ALL WARRANTIES AND CONDITIONS WITH REGARD TO THESE MATERIALS, INCLUDING BUT NOT LIMITED TO, ALL IMPLIED WARRANTIES AND CONDITIONS OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, TITLE AND NON-INFRINGEMENT OF ANY THIRD PARTY INTELLECTUAL PROPERTY RIGHT. NO LICENSE, EITHER EXPRESS OR IMPLIED, BY ESTOPPEL OR OTHERWISE, IS GRANTED BY TI. USE OF THE INFORMATION ON THIS SITE MAY REQUIRE A LICENSE FROM A THIRD PARTY, OR A LICENSE FROM TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI and its suppliers reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.